|
|
uint8_t | enableVal |
| |
|
uint8_t | padding [3] |
| |
|
uint8_t | index |
| |
|
uint32_t | value |
| |
|
uint8_t | rateVal |
| |
|
uint8_t | value |
| |
|
uint8_t | beaconRssi |
| |
|
uint8_t | overEnable |
| |
|
uint8_t | bw |
| |
|
uint8_t | preamble |
| |
|
uint8_t | rate |
| |
|
uint8_t | dcm |
| |
|
uint8_t | txPower |
| |
|
uint8_t | giLTF |
| |
|
uint32_t | receivedTotalPacketsNumber |
| |
|
uint32_t | receivedFcsErrorPacketsNumber |
| |
|
uint32_t | receivedAddressMismatchPacketsNumber |
| |
|
uint32_t | receivedGoodPackets |
| |
|
int16_t | averageDataCtrlRssi |
| |
|
int16_t | averageDataCtrlSNR |
| |
|
uint8_t | channel |
| |
|
uint8_t | band |
| |
|
uint8_t | bandwidth |
| |
|
uint32_t | bitmask |
| |
|
uint8_t | preambleType |
| |
|
uint8_t | phyRate |
| |
|
int8_t | txPower |
| |
|
uint8_t | GI_LTF_Type |
| |
|
uint8_t | DCM |
| |
|
uint16_t | startLength |
| |
|
uint16_t | endLength |
| |
|
uint32_t | delay |
| |
|
uint8_t | packetMode |
| |
|
uint16_t | numberOfPackets |
| |
|
uint8_t | dataMode |
| |
|
uint8_t | dataConstValue |
| |
|
uint8_t | enableCCA |
| |
|
uint8_t | bssColor |
| |
|
uint16_t | SU_ER_Bandwidth |
| |
|
uint8_t | partialAID |
| |
|
uint8_t | srcAddr [(6)] |
| |
|
uint8_t | dstAddr [(6)] |
| |
|
uint8_t | nominalPacketExtension |
| |
|
uint8_t | feedbackStatus |
| |
|
uint16_t | aid |
| |
|
uint8_t | groupId |
| |
|
uint8_t | ltfMode |
| |
|
uint8_t | heLtfNum |
| |
|
uint8_t | preFecPaddingFactor |
| |
|
uint16_t | commonInfoLen |
| |
|
uint16_t | ruAlloc |
| |
|
uint8_t | ulBw |
| |
|
uint8_t | startsStsNum |
| |
|
uint8_t | tbAutoMode |
| |
|
uint8_t | disamb |
| |
|
uint8_t | mode |
| |
|
int8_t | offset |
| |
|
int8_t | output_power |
| |
|
uint16_t | io_id |
| |
|
uint8_t | direction |
| |
|
uint8_t | state |
| |
|
uint8_t | ackEnable |
| |
|
uint8_t | macAddress [(6)] |
| |
|
uint8 | role_id |
| |
|
uint8 | pad [3] |
| |
|
uint32 | missed_beacons |
| |
|
uint8 | snr_data |
| |
|
uint8 | snr_beacon |
| |
|
int8 | rssi_data |
| |
|
int8 | rssi_beacon |
| |
The documentation for this struct was generated from the following file:
- .build.mcu/api-sources/thickmac/source/ti/drivers/net/wifi/wifi_host_driver/inc_adapt/wlan_if.h