CC33XX API Documentation  2.30.00.15
Public Attributes | List of all members
WlanPeer_t Struct Reference

Public Attributes

uint8_t * device_address
 
uint8_t connection_capability
 
uint32_t session_id
 
uint32_t advertisement_id
 
uint8_t * session_mac
 
uint8_t * adv_mac
 
uint8_t * persist_ssid
 
uint32_t persist_ssid_len
 
uint8_t dialog_token
 

The documentation for this struct was generated from the following file: