CC33XX API Documentation  2.30.00.15
Public Attributes | List of all members
WlanNetworkEntryExtended_t Struct Reference

Public Attributes

uint8_t Ssid [(32)]
 
uint8_t Bssid [(6)]
 
uint8_t SsidLen
 
int8_t Rssi
 
uint16_t SecurityInfo
 
uint8_t Channel
 
uint16_t mRatesLen
 
uint8_t mRates [(32)+(2)]
 
uint16_t HtCapabilitiesLen
 
uint8_t HtCapabilitiesIe [(26)+(2)]
 
uint16_t erpIeLen
 
uint8_t erpIe [(1)+(2)]
 
Bool_e mErpPresent
 
uint8_t mUseProtection
 
uint8_t mBarkerPreambleMode
 
uint8_t rsnIeLen
 
uint8_t rsnIeData [(257)+(2)]
 
uint8_t wpaIeLen
 
uint8_t wpaIeData [(257)+(2)]
 
uint16_t wpsLen
 
uint8_t wpsIeData [(350)+(2)]
 
Bool_e wpsPresent
 
uint16_t beaconInterval
 
uint16_t capabilities
 

The documentation for this struct was generated from the following file: