CC33XX API Documentation  2.30.00.15
Modules
Here is a list of all modules:
 upper MACThis module implements the user interface for the upper MAC
 init_adaptThis porting file provides the adaptation layer for the host interface
 spi_adaptThis porting file provides the adaptation layer for the host SPI interface
 osi_freertosThis porting file provides the adaptation layer for the OS
 osi_filesystemThis porting file provides the adaptation layer for the file system. These functions are needed for file management of the upper mac. Currently only supported file is the WiFi part firmware bin file. On the Sitara AM243x Launchpad, the firmware binary is saved in a specific flash offset