![]() |
![]() |
Configuration structure for PWM mode in the Timer_A module. See Timer_A_generatePWM for parameter documentation. More...
#include <timer_a.h>
Data Fields | |
| uint_fast16_t | clockSource |
| uint_fast16_t | clockSourceDivider |
| uint_fast16_t | timerPeriod |
| uint_fast16_t | compareRegister |
| uint_fast16_t | compareOutputMode |
| uint_fast16_t | dutyCycle |
Configuration structure for PWM mode in the Timer_A module. See Timer_A_generatePWM for parameter documentation.
| uint_fast16_t _Timer_A_PWMConfig::clockSource |
Referenced by Timer_A_generatePWM().
| uint_fast16_t _Timer_A_PWMConfig::clockSourceDivider |
Referenced by Timer_A_generatePWM().
| uint_fast16_t _Timer_A_PWMConfig::timerPeriod |
Referenced by Timer_A_generatePWM().
| uint_fast16_t _Timer_A_PWMConfig::compareRegister |
Referenced by Timer_A_generatePWM().
| uint_fast16_t _Timer_A_PWMConfig::compareOutputMode |
Referenced by Timer_A_generatePWM().
| uint_fast16_t _Timer_A_PWMConfig::dutyCycle |
Referenced by Timer_A_generatePWM().