![]() |
![]() |
Configuration structure for slave mode in the SPI module. See SPI_initSlave for parameter documentation. More...
#include <spi.h>
Data Fields | |
| uint_fast16_t | msbFirst |
| uint_fast16_t | clockPhase |
| uint_fast16_t | clockPolarity |
| uint_fast16_t | spiMode |
Configuration structure for slave mode in the SPI module. See SPI_initSlave for parameter documentation.
| uint_fast16_t _SPI_SlaveConfig::msbFirst |
Referenced by SPI_initSlave().
| uint_fast16_t _SPI_SlaveConfig::clockPhase |
Referenced by SPI_initSlave().
| uint_fast16_t _SPI_SlaveConfig::clockPolarity |
Referenced by SPI_initSlave().
| uint_fast16_t _SPI_SlaveConfig::spiMode |
Referenced by SPI_initSlave().