|
| bool | SPI_initMaster (uint32_t moduleInstance, const SPI_MasterConfig *config) |
| |
| void | SPI_selectFourPinFunctionality (uint32_t moduleInstance, uint_fast8_t select4PinFunctionality) |
| |
| void | SPI_changeMasterClock (uint32_t moduleInstance, uint32_t clockSourceFrequency, uint32_t desiredSpiClock) |
| |
| bool | SPI_initSlave (uint32_t moduleInstance, const SPI_SlaveConfig *config) |
| |
| void | SPI_changeClockPhasePolarity (uint32_t moduleInstance, uint_fast16_t clockPhase, uint_fast16_t clockPolarity) |
| |
| void | SPI_transmitData (uint32_t moduleInstance, uint_fast8_t transmitData) |
| |
| uint8_t | SPI_receiveData (uint32_t moduleInstance) |
| |
| void | SPI_enableModule (uint32_t moduleInstance) |
| |
| void | SPI_disableModule (uint32_t moduleInstance) |
| |
| uint32_t | SPI_getReceiveBufferAddressForDMA (uint32_t moduleInstance) |
| |
| uint32_t | SPI_getTransmitBufferAddressForDMA (uint32_t moduleInstance) |
| |
| uint_fast8_t | SPI_isBusy (uint32_t moduleInstance) |
| |
| void | SPI_enableInterrupt (uint32_t moduleInstance, uint_fast8_t mask) |
| |
| void | SPI_disableInterrupt (uint32_t moduleInstance, uint_fast8_t mask) |
| |
| uint_fast8_t | SPI_getInterruptStatus (uint32_t moduleInstance) |
| |
| uint_fast8_t | SPI_getEnabledInterruptStatus (uint32_t moduleInstance) |
| |
| void | SPI_clearInterruptFlag (uint32_t moduleInstance, uint_fast8_t mask) |
| |
| void | SPI_registerInterrupt (uint32_t moduleInstance, void(*intHandler)(void)) |
| |
| void | SPI_unregisterInterrupt (uint32_t moduleInstance) |
| |
| void | EUSCI_A_SPI_select4PinFunctionality (uint32_t baseAddress, uint8_t select4PinFunctionality) |
| | Selects 4Pin Functionality. More...
|
| |
| void | EUSCI_A_SPI_masterChangeClock (uint32_t baseAddress, uint32_t clockSourceFrequency, uint32_t desiredSpiClock) |
| | Initializes the SPI Master clock. At the end of this function call, SPI module is left enabled. More...
|
| |
| bool | EUSCI_A_SPI_slaveInit (uint32_t baseAddress, uint16_t msbFirst, uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode) |
| | Initializes the SPI Slave block. More...
|
| |
| void | EUSCI_A_SPI_changeClockPhasePolarity (uint32_t baseAddress, uint16_t clockPhase, uint16_t clockPolarity) |
| | Changes the SPI colock phase and polarity. At the end of this function call, SPI module is left enabled. More...
|
| |
| void | EUSCI_A_SPI_transmitData (uint32_t baseAddress, uint8_t transmitData) |
| | Transmits a byte from the SPI Module. More...
|
| |
| uint8_t | EUSCI_A_SPI_receiveData (uint32_t baseAddress) |
| | Receives a byte that has been sent to the SPI Module. More...
|
| |
| void | EUSCI_A_SPI_enableInterrupt (uint32_t baseAddress, uint8_t mask) |
| | Enables individual SPI interrupt sources. More...
|
| |
| void | EUSCI_A_SPI_disableInterrupt (uint32_t baseAddress, uint8_t mask) |
| | Disables individual SPI interrupt sources. More...
|
| |
| uint8_t | EUSCI_A_SPI_getInterruptStatus (uint32_t baseAddress, uint8_t mask) |
| | Gets the current SPI interrupt status. More...
|
| |
| void | EUSCI_A_SPI_clearInterruptFlag (uint32_t baseAddress, uint8_t mask) |
| | Clears the selected SPI interrupt status flag. More...
|
| |
| void | EUSCI_A_SPI_enable (uint32_t baseAddress) |
| | Enables the SPI block. More...
|
| |
| void | EUSCI_A_SPI_disable (uint32_t baseAddress) |
| | Disables the SPI block. More...
|
| |
| uint32_t | EUSCI_A_SPI_getReceiveBufferAddressForDMA (uint32_t baseAddress) |
| | Returns the address of the RX Buffer of the SPI for the DMA module. More...
|
| |
| uint32_t | EUSCI_A_SPI_getTransmitBufferAddressForDMA (uint32_t baseAddress) |
| | Returns the address of the TX Buffer of the SPI for the DMA module. More...
|
| |
| bool | EUSCI_A_SPI_isBusy (uint32_t baseAddress) |
| | Indicates whether or not the SPI bus is busy. More...
|
| |
| void | EUSCI_B_SPI_select4PinFunctionality (uint32_t baseAddress, uint8_t select4PinFunctionality) |
| | Selects 4Pin Functionality. More...
|
| |
| void | EUSCI_B_SPI_masterChangeClock (uint32_t baseAddress, uint32_t clockSourceFrequency, uint32_t desiredSpiClock) |
| | Initializes the SPI Master clock. At the end of this function call, SPI module is left enabled. More...
|
| |
| bool | EUSCI_B_SPI_slaveInit (uint32_t baseAddress, uint16_t msbFirst, uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode) |
| | Initializes the SPI Slave block. More...
|
| |
| void | EUSCI_B_SPI_changeClockPhasePolarity (uint32_t baseAddress, uint16_t clockPhase, uint16_t clockPolarity) |
| | Changes the SPI colock phase and polarity. At the end of this function call, SPI module is left enabled. More...
|
| |
| void | EUSCI_B_SPI_transmitData (uint32_t baseAddress, uint8_t transmitData) |
| | Transmits a byte from the SPI Module. More...
|
| |
| uint8_t | EUSCI_B_SPI_receiveData (uint32_t baseAddress) |
| | Receives a byte that has been sent to the SPI Module. More...
|
| |
| void | EUSCI_B_SPI_enableInterrupt (uint32_t baseAddress, uint8_t mask) |
| | Enables individual SPI interrupt sources. More...
|
| |
| void | EUSCI_B_SPI_disableInterrupt (uint32_t baseAddress, uint8_t mask) |
| | Disables individual SPI interrupt sources. More...
|
| |
| uint8_t | EUSCI_B_SPI_getInterruptStatus (uint32_t baseAddress, uint8_t mask) |
| | Gets the current SPI interrupt status. More...
|
| |
| void | EUSCI_B_SPI_clearInterruptFlag (uint32_t baseAddress, uint8_t mask) |
| | Clears the selected SPI interrupt status flag. More...
|
| |
| void | EUSCI_B_SPI_enable (uint32_t baseAddress) |
| | Enables the SPI block. More...
|
| |
| void | EUSCI_B_SPI_disable (uint32_t baseAddress) |
| | Disables the SPI block. More...
|
| |
| uint32_t | EUSCI_B_SPI_getReceiveBufferAddressForDMA (uint32_t baseAddress) |
| | Returns the address of the RX Buffer of the SPI for the DMA module. More...
|
| |
| uint32_t | EUSCI_B_SPI_getTransmitBufferAddressForDMA (uint32_t baseAddress) |
| | Returns the address of the TX Buffer of the SPI for the DMA module. More...
|
| |
| bool | EUSCI_B_SPI_isBusy (uint32_t baseAddress) |
| | Indicates whether or not the SPI bus is busy. More...
|
| |