Real Time Clock with alarm support and tamper protection.
More...
|
| #define | RTC_C_CALIBRATIONFREQ_OFF (RTCCALF_0) |
| |
| #define | RTC_C_CALIBRATIONFREQ_512HZ (RTCCALF_1) |
| |
| #define | RTC_C_CALIBRATIONFREQ_256HZ (RTCCALF_2) |
| |
| #define | RTC_C_CALIBRATIONFREQ_1HZ (RTCCALF_3) |
| |
| #define | RTC_C_CALIBRATION_DOWN1PPM ( !(RTCOCALS) ) |
| |
| #define | RTC_C_CALIBRATION_UP1PPM (RTCOCALS) |
| |
| #define | RTC_C_COMPENSATION_DOWN1PPM ( !(RTCTCMPS) ) |
| |
| #define | RTC_C_COMPENSATION_UP1PPM (RTCTCMPS) |
| |
| #define | RTC_C_FORMAT_BINARY ( !(RTCBCD) ) |
| |
| #define | RTC_C_FORMAT_BCD (RTCBCD) |
| |
| #define | RTC_C_ALARMCONDITION_OFF (0x80) |
| |
| #define | RTC_C_CALENDAREVENT_MINUTECHANGE (RTCTEV_0) |
| |
| #define | RTC_C_CALENDAREVENT_HOURCHANGE (RTCTEV_1) |
| |
| #define | RTC_C_CALENDAREVENT_NOON (RTCTEV_2) |
| |
| #define | RTC_C_CALENDAREVENT_MIDNIGHT (RTCTEV_3) |
| |
| #define | RTC_C_PRESCALE_0 (0x0) |
| |
| #define | RTC_C_PRESCALE_1 (0x1) |
| |
| #define | RTC_C_PSEVENTDIVIDER_2 (RT0IP_0) |
| |
| #define | RTC_C_PSEVENTDIVIDER_4 (RT0IP_1) |
| |
| #define | RTC_C_PSEVENTDIVIDER_8 (RT0IP_2) |
| |
| #define | RTC_C_PSEVENTDIVIDER_16 (RT0IP_3) |
| |
| #define | RTC_C_PSEVENTDIVIDER_32 (RT0IP_4) |
| |
| #define | RTC_C_PSEVENTDIVIDER_64 (RT0IP_5) |
| |
| #define | RTC_C_PSEVENTDIVIDER_128 (RT0IP_6) |
| |
| #define | RTC_C_PSEVENTDIVIDER_256 (RT0IP_7) |
| |
| #define | RTC_C_OSCILLATOR_FAULT_INTERRUPT RTCOFIE |
| |
| #define | RTC_C_TIME_EVENT_INTERRUPT RTCTEVIE |
| |
| #define | RTC_C_CLOCK_ALARM_INTERRUPT RTCAIE |
| |
| #define | RTC_C_CLOCK_READ_READY_INTERRUPT RTCRDYIE |
| |
| #define | RTC_C_PRESCALE_TIMER0_INTERRUPT 0x02 |
| |
| #define | RTC_C_PRESCALE_TIMER1_INTERRUPT 0x01 |
| |
| #define | RTC_C_startClockMultipleInstance(a) RTC_C_startClock() |
| |
| #define | RTC_C_holdClockMultipleInstance(a) RTC_C_holdClock() |
| |
| #define | RTC_C_setCalibrationFrequencyMultipleInstance(a, b) RTC_C_setCalibrationFrequency(b) |
| |
| #define | RTC_C_setCalibrationDataMultipleInstance(a, b, c) RTC_C_setCalibrationData(b,c) |
| |
| #define | RTC_C_setTemperatureCompensationMultipleInstance(a, b, c) RTC_C_setTemperatureCompensation(b,c) |
| |
| #define | RTC_C_initCalendarMultipleInstance(a, b, c) RTC_C_initCalendar(b,c) |
| |
| #define | RTC_C_getCalendarTimeMultipleInstance(a) RTC_C_getCalendarTime() |
| |
| #define | RTC_C_setCalendarAlarmMultipleInstance(a, b, c, d, e) RTC_C_setCalendarAlarm(b,c,d,e) |
| |
| #define | RTC_C_setCalendarEventMultipleInstance(a, b) RTC_C_setCalendarEvent(b) |
| |
| #define | RTC_C_definePrescaleEventMultipleInstance(a, b, c) RTC_C_definePrescaleEvent(b,c) |
| |
| #define | RTC_C_getPrescaleValueMultipleInstance(a, b) RTC_C_getPrescaleValue(b) |
| |
| #define | RTC_C_setPrescaleValueMultipleInstance(a, b, c) RTC_C_setPrescaleValue(b,c) |
| |
| #define | RTC_C_convertBCDToBinaryMultipleInstance(a, b) RTC_C_convertBCDToBinary(b) |
| |
| #define | RTC_C_convertBinaryToBCDMultipleInstance(a, b) RTC_C_convertBinaryToBCD(b) |
| |
| #define | RTC_C_enableInterruptMultipleInstance(a, b) RTC_C_enableInterrupt(b) |
| |
| #define | RTC_C_disableInterruptMultipleInstance(a, b) RTC_C_disableInterrupt(b) |
| |
| #define | RTC_C_getInterruptStatusMultipleInstance(a) RTC_C_getInterruptStatus() |
| |
| #define | RTC_C_getEnabledInterruptStatusMultipleInstance(a) RTC_C_getEnabledInterruptStatus() |
| |
| #define | RTC_C_clearInterruptFlagMultipleInstance(a, b) RTC_C_clearInterruptFlag(b) |
| |
| #define | RTC_C_registerInterruptMultipleInstance(a, b) RTC_C_registerInterrupt(b) |
| |
| #define | RTC_C_unregisterInterruptMultipleInstance(a) RTC_C_unregisterInterrupt() |
| |
Real Time Clock with alarm support and tamper protection.
Module Operation
The Real Time Clock (RTC) API provides a set of functions for using the MSPWare L RTC modules. Functions are provided to calibrate the clock, initialize the RTC modules in Calendar mode, and setup conditions for, and enable, interrupts for the RTC modules.
The RTC module provides the ability to keep track of the current time and date in calendar mode.
The RTC module generates multiple interrupts. There are 2 interrupts that can be defined in calendar mode, and 1 interrupt in counter mode for counter overflow, as well as an interrupt for each prescaler.
Programming Example
The DriverLib package contains a variety of different code examples that demonstrate the usage of the RTC module. These code examples are accessible under the examples/ folder of the MSPWare release as well as through TI Resource Explorer if using Code Composer Studio. These code examples provide a comprehensive list of use cases as well as practical applications involving each module.
Below is a very brief code example showing how to configure the RTC module and create a calendar event.
The following is the configuration structure that sets the date:
{
0x00,
0x03,
0x22,
0x12,
0x11,
0x1955
};
Next are the actual calls to DriverLib that configure the module:
| #define RTC_C_CALIBRATIONFREQ_OFF (RTCCALF_0) |
| #define RTC_C_CALIBRATIONFREQ_512HZ (RTCCALF_1) |
| #define RTC_C_CALIBRATIONFREQ_256HZ (RTCCALF_2) |
| #define RTC_C_CALIBRATIONFREQ_1HZ (RTCCALF_3) |
| #define RTC_C_CALIBRATION_DOWN1PPM ( !(RTCOCALS) ) |
| #define RTC_C_CALIBRATION_UP1PPM (RTCOCALS) |
| #define RTC_C_COMPENSATION_DOWN1PPM ( !(RTCTCMPS) ) |
| #define RTC_C_COMPENSATION_UP1PPM (RTCTCMPS) |
| #define RTC_C_FORMAT_BINARY ( !(RTCBCD) ) |
| #define RTC_C_FORMAT_BCD (RTCBCD) |
| #define RTC_C_ALARMCONDITION_OFF (0x80) |
| #define RTC_C_CALENDAREVENT_MINUTECHANGE (RTCTEV_0) |
| #define RTC_C_CALENDAREVENT_HOURCHANGE (RTCTEV_1) |
| #define RTC_C_CALENDAREVENT_NOON (RTCTEV_2) |
| #define RTC_C_CALENDAREVENT_MIDNIGHT (RTCTEV_3) |
| #define RTC_C_PRESCALE_0 (0x0) |
| #define RTC_C_PRESCALE_1 (0x1) |
| #define RTC_C_PSEVENTDIVIDER_2 (RT0IP_0) |
| #define RTC_C_PSEVENTDIVIDER_4 (RT0IP_1) |
| #define RTC_C_PSEVENTDIVIDER_8 (RT0IP_2) |
| #define RTC_C_PSEVENTDIVIDER_16 (RT0IP_3) |
| #define RTC_C_PSEVENTDIVIDER_32 (RT0IP_4) |
| #define RTC_C_PSEVENTDIVIDER_64 (RT0IP_5) |
| #define RTC_C_PSEVENTDIVIDER_128 (RT0IP_6) |
| #define RTC_C_PSEVENTDIVIDER_256 (RT0IP_7) |
| #define RTC_C_OSCILLATOR_FAULT_INTERRUPT RTCOFIE |
| #define RTC_C_TIME_EVENT_INTERRUPT RTCTEVIE |
| #define RTC_C_CLOCK_ALARM_INTERRUPT RTCAIE |
| #define RTC_C_CLOCK_READ_READY_INTERRUPT RTCRDYIE |
| #define RTC_C_PRESCALE_TIMER0_INTERRUPT 0x02 |
| #define RTC_C_PRESCALE_TIMER1_INTERRUPT 0x01 |
| void RTC_C_startClock |
( |
void |
| ) |
|
Starts the RTC.
This function clears the RTC main hold bit to allow the RTC to function.
- Returns
- None
References RTCKEY_H.
| void RTC_C_holdClock |
( |
void |
| ) |
|
Holds the RTC.
This function sets the RTC main hold bit to disable RTC functionality.
- Returns
- None
References RTCKEY_H.
| void RTC_C_setCalibrationFrequency |
( |
uint_fast16_t |
frequencySelect | ) |
|
Allows and Sets the frequency output to RTCLK pin for calibration measurement.
- Parameters
-
| frequencySelect | is the frequency output to RTCLK. Valid values are
- RTC_C_CALIBRATIONFREQ_OFF - turn off calibration output [Default]
- RTC_C_CALIBRATIONFREQ_512HZ - output signal at 512Hz for calibration
- RTC_C_CALIBRATIONFREQ_256HZ - output signal at 256Hz for calibration
- RTC_C_CALIBRATIONFREQ_1HZ - output signal at 1Hz for calibration
|
This function sets a frequency to measure at the RTCLK output pin. After testing the set frequency, the calibration could be set accordingly.
- Returns
- None
References RTCKEY_H.
| void RTC_C_setCalibrationData |
( |
uint_fast8_t |
offsetDirection, |
|
|
uint_fast8_t |
offsetValue |
|
) |
| |
Sets the specified calibration for the RTC.
- Parameters
-
| offsetDirection | is the direction that the calibration offset will go. Valid values are
- RTC_C_CALIBRATION_DOWN1PPM - calibrate at steps of -1
- RTC_C_CALIBRATION_UP1PPM - calibrat at steps of +1
|
| offsetValue | is the value that the offset will be a factor of; a valid value is any integer from 1-240. |
This function sets the calibration offset to make the RTC as accurate as possible. The offsetDirection can be either +1-ppm or -1-ppm, and the offsetValue should be from 1-240 and is multiplied by the direction setting (i.e. +1-ppm * 8 (offsetValue) = +8-ppm).
- Returns
- None
References RTCKEY_H.
| bool RTC_C_setTemperatureCompensation |
( |
uint_fast16_t |
offsetDirection, |
|
|
uint_fast8_t |
offsetValue |
|
) |
| |
Sets the specified temperature compensation for the RTC.
- Parameters
-
| offsetDirection | is the direction that the calibration offset will go. Valid values are
- RTC_C_COMPENSATION_DOWN1PPM - calibrate at steps of -1
- RTC_C_COMPENSATION_UP1PPM - calibrate at steps of +1
|
| offsetValue | is the value that the offset will be a factor of; a value is any integer from 1-240. |
This function sets the calibration offset to make the RTC as accurate as possible. The offsetDirection can be either +1-ppm or -1-ppm, and the offsetValue should be from 1-240 and is multiplied by the direction setting (i.e. +1-ppm * 8 (offsetValue) = +8-ppm).
- Returns
- true if calibration was set, false if it could not be set
| void RTC_C_initCalendar |
( |
const RTC_C_Calendar * |
calendarTime, |
|
|
uint_fast16_t |
formatSelect |
|
) |
| |
Initializes the settings to operate the RTC in Calendar mode.
- Parameters
-
| calendarTime | is the structure containing the values for the Calendar to be initialized to. Valid values should be of type Calendar and should contain the following members and corresponding values:
- seconds between 0-59
- minutes between 0-59
- hours between 0-24
- dayOfWeek between 0-6
- dayOfmonth between 0-31
- year between 0-4095
|
- Note
- Values beyond the ones specified may result in eradic behavior.
- Parameters
-
| formatSelect | is the format for the Calendar registers to use. Valid values are
- RTC_FORMAT_BINARY [Default]
- RTC_FORMAT_BCD
|
This function initializes the Calendar mode of the RTC module.
- Returns
- None
References _RTC_C_Calendar::dayOfmonth, _RTC_C_Calendar::dayOfWeek, _RTC_C_Calendar::hours, _RTC_C_Calendar::minutes, _RTC_C_Calendar::month, RTCKEY_H, _RTC_C_Calendar::seconds, and _RTC_C_Calendar::year.
| void RTC_C_setCalendarAlarm |
( |
uint_fast8_t |
minutesAlarm, |
|
|
uint_fast8_t |
hoursAlarm, |
|
|
uint_fast8_t |
dayOfWeekAlarm, |
|
|
uint_fast8_t |
dayOfmonthAlarm |
|
) |
| |
Sets and Enables the desired Calendar Alarm settings.
- Parameters
-
| minutesAlarm | is the alarm condition for the minutes. Valid values are
- An integer between 0-59, OR
- RTC_C_ALARMCONDITION_OFF [Default]
|
| hoursAlarm | is the alarm condition for the hours. Valid values are
- An integer between 0-24, OR
- RTC_C_ALARMCONDITION_OFF [Default]
|
| dayOfWeekAlarm | is the alarm condition for the day of week. Valid values are
- An integer between 0-6, OR
- RTC_C_ALARMCONDITION_OFF [Default]
|
| dayOfmonthAlarm | is the alarm condition for the day of the month. Valid values are
- An integer between 0-31, OR
- RTC_C_ALARMCONDITION_OFF [Default]
|
This function sets a Calendar interrupt condition to assert the RTCAIFG interrupt flag. The condition is a logical and of all of the parameters. For example if the minutes and hours alarm is set, then the interrupt will only assert when the minutes AND the hours change to the specified setting. Use the RTC_ALARM_OFF for any alarm settings that should not be apart of the alarm condition.
- Returns
- None
References __RTC_C_BASE__, OFS_RTCADOWDAY_H, OFS_RTCADOWDAY_L, OFS_RTCAMINHR_H, and OFS_RTCAMINHR_L.
| void RTC_C_setCalendarEvent |
( |
uint_fast16_t |
eventSelect | ) |
|
Sets a single specified Calendar interrupt condition.
- Parameters
-
| eventSelect | is the condition selected. Valid values are
- RTC_C_CALENDAREVENT_MINUTECHANGE - assert interrupt on every minute
- RTC_C_CALENDAREVENT_HOURCHANGE - assert interrupt on every hour
- RTC_C_CALENDAREVENT_NOON - assert interrupt when hour is 12
- RTC_C_CALENDAREVENT_MIDNIGHT - assert interrupt when hour is 0
|
This function sets a specified event to assert the RTCTEVIFG interrupt. This interrupt is independent from the Calendar alarm interrupt.
- Returns
- None
References RTCKEY_H.
| void RTC_C_definePrescaleEvent |
( |
uint_fast8_t |
prescaleSelect, |
|
|
uint_fast8_t |
prescaleEventDivider |
|
) |
| |
Sets up an interrupt condition for the selected Prescaler.
- Parameters
-
| prescaleSelect | is the prescaler to define an interrupt for. Valid values are
- RTC_C_PRESCALE_0
- RTC_C_PRESCALE_1
|
| prescaleEventDivider | is a divider to specify when an interrupt can occur based on the clock source of the selected prescaler. (Does not affect timer of the selected prescaler). Valid values are
- RTC_C_PSEVENTDIVIDER_2 [Default]
- RTC_C_PSEVENTDIVIDER_4
- RTC_C_PSEVENTDIVIDER_8
- RTC_C_PSEVENTDIVIDER_16
- RTC_C_PSEVENTDIVIDER_32
- RTC_C_PSEVENTDIVIDER_64
- RTC_C_PSEVENTDIVIDER_128
- RTC_C_PSEVENTDIVIDER_256
|
This function sets the condition for an interrupt to assert based on the individual prescalers.
- Returns
- None
References __RTC_C_BASE__, and OFS_RTCPS0CTL_L.
| uint_fast8_t RTC_C_getPrescaleValue |
( |
uint_fast8_t |
prescaleSelect | ) |
|
Returns the selected Prescaler value.
- Parameters
-
| prescaleSelect | is the prescaler to obtain the value of. Valid values are
- RTC_C_PRESCALE_0
- RTC_C_PRESCALE_1
|
This function returns the value of the selected prescale counter register. The counter should be held before reading. If in counter mode, the individual prescaler can be held, while in Calendar mode the whole RTC must be held.
- Returns
- The value of the specified Prescaler count register
References RTC_C_PRESCALE_0, and RTC_C_PRESCALE_1.
| void RTC_C_setPrescaleValue |
( |
uint_fast8_t |
prescaleSelect, |
|
|
uint_fast8_t |
prescaleCounterValue |
|
) |
| |
Sets the selected Prescaler value.
- Parameters
-
| prescaleSelect | is the prescaler to set the value for. Valid values are
- RTC_C_PRESCALE_0
- RTC_C_PRESCALE_1
|
| prescaleCounterValue | is the specified value to set the prescaler to; a valid value is any integer from 0-255. |
This function sets the prescale counter value. Before setting the prescale counter, it should be held.
- Returns
- None
References RTC_C_PRESCALE_0, RTC_C_PRESCALE_1, and RTCKEY_H.
| uint16_t RTC_C_convertBCDToBinary |
( |
uint16_t |
valueToConvert | ) |
|
Returns the given BCD value in Binary Format
- Parameters
-
| valueToConvert | is the raw value in BCD format to convert to Binary. |
This function converts BCD values to Binary format.
- Returns
- The Binary version of the valueToConvert parameter.
| uint16_t RTC_C_convertBinaryToBCD |
( |
uint16_t |
valueToConvert | ) |
|
Returns the given Binary value in BCD Format
- Parameters
-
| valueToConvert | is the raw value in Binary format to convert to BCD. |
This function converts Binary values to BCD format.
- Returns
- The BCD version of the valueToConvert parameter.
| void RTC_C_enableInterrupt |
( |
uint8_t |
interruptMask | ) |
|
Enables selected RTC interrupt sources.
- Parameters
-
| interruptMask | is a bit mask of the interrupts to enable. Mask Value is the logical OR of any of the following
- RTC_C_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by defineCalendarEvent() is met.
- RTC_C_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.
- RTC_C_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.
- RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.
- RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.
- RTC_C_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running.
|
This function enables the selected RTC interrupt source. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
- Returns
- None
References RTC_C_PRESCALE_TIMER0_INTERRUPT, RTC_C_PRESCALE_TIMER1_INTERRUPT, and RTCKEY.
| void RTC_C_disableInterrupt |
( |
uint8_t |
interruptMask | ) |
|
Disables selected RTC interrupt sources.
- Parameters
-
| interruptMask | is a bit mask of the interrupts to disable. Mask Value is the logical OR of any of the following
- RTC_C_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by defineCalendarEvent() is met.
- RTC_C_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.
- RTC_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.
- RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.
- RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.
- RTC_C_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running.
|
This function disables the selected RTC interrupt source. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
- Returns
- None
References RTC_C_PRESCALE_TIMER0_INTERRUPT, RTC_C_PRESCALE_TIMER1_INTERRUPT, and RTCKEY.
| uint_fast8_t RTC_C_getInterruptStatus |
( |
void |
| ) |
|
| uint_fast8_t RTC_C_getEnabledInterruptStatus |
( |
void |
| ) |
|
Returns the status of the interrupts flags masked with the enabled interrupts. This function is useful to call in ISRs to get a list of pending interrupts that are actually enabled and could have caused the ISR.
- Returns
- A bit mask of the selected interrupt flag's status. Mask Value is the logical OR of any of the following
- RTC_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by defineCalendarEvent() is met.
- RTC_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.
- RTC_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.
- RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.
- RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.
- RTC_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running.
References RTC_C_CLOCK_ALARM_INTERRUPT, RTC_C_CLOCK_READ_READY_INTERRUPT, RTC_C_getInterruptStatus(), RTC_C_OSCILLATOR_FAULT_INTERRUPT, RTC_C_PRESCALE_TIMER0_INTERRUPT, RTC_C_PRESCALE_TIMER1_INTERRUPT, and RTC_C_TIME_EVENT_INTERRUPT.
| void RTC_C_clearInterruptFlag |
( |
uint_fast8_t |
interruptFlagMask | ) |
|
Clears selected RTC interrupt flags.
- Parameters
-
| interruptFlagMask | is a bit mask of the interrupt flags to be cleared. Mask Value is the logical OR of any of the following
- RTC_C_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by defineCalendarEvent() is met.
- RTC_C_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.
- RTC_C_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.
- RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.
- RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.
- RTC_C_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running.
|
This function clears the RTC interrupt flag is cleared, so that it no longer asserts.
- Returns
- None
References RTC_C_CLOCK_ALARM_INTERRUPT, RTC_C_CLOCK_READ_READY_INTERRUPT, RTC_C_OSCILLATOR_FAULT_INTERRUPT, RTC_C_PRESCALE_TIMER0_INTERRUPT, RTC_C_PRESCALE_TIMER1_INTERRUPT, RTC_C_TIME_EVENT_INTERRUPT, and RTCKEY.
| void RTC_C_registerInterrupt |
( |
void(*)(void) |
intHandler | ) |
|
Registers an interrupt handler for the RTC interrupt.
- Parameters
-
| intHandler | is a pointer to the function to be called when the RTC interrupt occurs. |
This function registers the handler to be called when a RTC interrupt occurs. This function enables the global interrupt in the interrupt controller; specific AES interrupts must be enabled via RTC_enableInterrupt(). It is the interrupt handler's responsibility to clear the interrupt source via RTC_clearInterruptFlag().
- Returns
- None.
References Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().
| void RTC_C_unregisterInterrupt |
( |
void |
| ) |
|
Unregisters the interrupt handler for the RTC interrupt
This function unregisters the handler to be called when RTC interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
- See also
- Interrupt_registerInterrupt() for important information about registering interrupt handlers.
- Returns
- None.
References Interrupt_disableInterrupt(), and Interrupt_unregisterInterrupt().