![]() |
![]() |
Reference module used to create/configure analog voltage reference. More...
Functions | |
| void | REF_A_setReferenceVoltage (uint_fast8_t referenceVoltageSelect) |
| void | REF_A_disableTempSensor (void) |
| void | REF_A_enableTempSensor (void) |
| void | REF_A_enableReferenceVoltageOutput (void) |
| void | REF_A_disableReferenceVoltageOutput (void) |
| void | REF_A_enableReferenceVoltage (void) |
| void | REF_A_disableReferenceVoltage (void) |
| uint_fast8_t | REF_A_getBandgapMode (void) |
| bool | REF_A_isBandgapActive (void) |
| bool | REF_A_isRefGenBusy (void) |
| bool | REF_A_isRefGenActive (void) |
| bool | REF_A_getBufferedBandgapVoltageStatus (void) |
| bool | REF_A_getVariableReferenceVoltageStatus (void) |
| void | REF_A_setReferenceVoltageOneTimeTrigger (void) |
| void | REF_A_setBufferedBandgapVoltageOneTimeTrigger (void) |
Reference module used to create/configure analog voltage reference.
Below is a very brief code example showing how to enable the REF module for a 2.5v reference:
| #define REF_A_VREF1_2V REFVSEL_0 |
| #define REF_A_VREF1_45V REFVSEL_1 |
| #define REF_A_VREF2_0V REFVSEL_2 |
| #define REF_A_VREF2_5V REFVSEL_3 |
Referenced by REF_A_setReferenceVoltage().
| #define REF_A_STATICMODE 0x0 |
| #define REF_A_SAMPLEMODE BGMODE |
| #define REF_A_setReferenceVoltageMultipleInstance | ( | a, | |
| b | |||
| ) | REF_A_setReferenceVoltage(b) |
| #define REF_A_disableTempSensorMultipleInstance | ( | a | ) | REF_A_disableTempSensor() |
| #define REF_A_enableTempSensorMultipleInstance | ( | a | ) | REF_A_enableTempSensor() |
| #define REF_A_enableReferenceVoltageOutputMultipleInstance | ( | a | ) | REF_A_enableReferenceVoltageOutput() |
| #define REF_A_disableReferenceVoltageOutputMultipleInstance | ( | a | ) | REF_A_disableReferenceVoltageOutput() |
| #define REF_A_enableReferenceVoltageMultipleInstance | ( | a | ) | REF_A_enableReferenceVoltage() |
| #define REF_A_disableReferenceVoltageMultipleInstance | ( | a | ) | REF_A_disableReferenceVoltage() |
| #define REF_A_getBandgapModeMultipleInstance | ( | a | ) | REF_A_getBandgapMode() |
| #define REF_A_isBandgapActiveMultipleInstance | ( | a | ) | REF_A_isBandgapActive() |
| #define REF_A_isRefGenBusyMultipleInstance | ( | a | ) | REF_A_isRefGenBusy() |
| #define REF_A_isRefGenActiveMultipleInstance | ( | a | ) | REF_A_isRefGenActive() |
| #define REF_A_getBufferedBandgapVoltageStatusMultipleInstance | ( | a | ) | REF_A_getBufferedBandgapVoltageStatus() |
| #define REF_A_getVariableReferenceVoltageStatusMultipleInstance | ( | a | ) | REF_A_getVariableReferenceVoltageStatus() |
| #define REF_A_setReferenceVoltageOneTimeTriggerMultipleInstance | ( | a | ) | REF_A_setReferenceVoltageOneTimeTrigger() |
| #define REF_A_setBufferedBandgapVoltageOneTimeTriggerMultipleInstance | ( | a | ) | REF_A_setBufferedBandgapVoltageOneTimeTrigger() |
| void REF_A_setReferenceVoltage | ( | uint_fast8_t | referenceVoltageSelect | ) |
Sets the reference voltage for the voltage generator.
| referenceVoltageSelect | is the desired voltage to generate for a reference voltage. Valid values are:
|
This function sets the reference voltage generated by the voltage generator to be used by other peripherals. This reference voltage will only be valid while the REF module is in control. Please note, if the REF_A_isRefGenBusy() returns REF_BUSY, this function will have no effect.
References ASSERT, and REF_A_VREF2_5V.
| void REF_A_disableTempSensor | ( | void | ) |
Disables the internal temperature sensor to save power consumption.
This function is used to turn off the internal temperature sensor to save on power consumption. The temperature sensor is enabled by default. Please note, that giving ADC12 module control over the REF module, the state of the temperature sensor is dependent on the controls of the ADC12 module. Please note, if the REF_A_isRefGenBusy() returns REF_A_BUSY, this function will have no effect.
Modified bits are REFTCOFF of REFCTL0 register.
| void REF_A_enableTempSensor | ( | void | ) |
Enables the internal temperature sensor.
This function is used to turn on the internal temperature sensor to use by other peripherals. The temperature sensor is enabled by default. Please note, if the REF_A_isRefGenBusy() returns REF_A_BUSY, this function will have no effect.
Modified bits are REFTCOFF of REFCTL0 register.
| void REF_A_enableReferenceVoltageOutput | ( | void | ) |
Outputs the reference voltage to an output pin.
This function is used to output the reference voltage being generated to an output pin. Please note, the output pin is device specific. Please note, that giving ADC12 module control over the REF module, the state of the reference voltage as an output to a pin is dependent on the controls of the ADC12 module. Please note, if the REF_A_isRefGenBusy() returns REF_A_BUSY, this function will have no effect.
Modified bits are REFOUT of REFCTL0 register.
| void REF_A_disableReferenceVoltageOutput | ( | void | ) |
Disables the reference voltage as an output to a pin.
This function is used to disables the reference voltage being generated to be given to an output pin. Please note, if the REF_A_isRefGenBusy() returns REF_A_BUSY, this function will have no effect.
Modified bits are REFOUT of REFCTL0 register.
| void REF_A_enableReferenceVoltage | ( | void | ) |
Enables the reference voltage to be used by peripherals.
This function is used to enable the generated reference voltage to be used other peripherals or by an output pin, if enabled. Please note, that giving ADC12 module control over the REF module, the state of the reference voltage is dependent on the controls of the ADC12 module. Please note, if the REF_A_isRefGenBusy() returns REF_A_BUSY, this function will have no effect.
Modified bits are REFON of REFCTL0 register.
| void REF_A_disableReferenceVoltage | ( | void | ) |
Disables the reference voltage.
This function is used to disable the generated reference voltage. Please note, if the REF_A_isRefGenBusy() returns REF_A_BUSY, this function will have no effect.
Modified bits are REFON of REFCTL0 register.
| uint_fast8_t REF_A_getBandgapMode | ( | void | ) |
Returns the bandgap mode of the REF module.
This function is used to return the bandgap mode of the REF module, requested by the peripherals using the bandgap. If a peripheral requests static mode, then the bandgap mode will be static for all modules, whereas if all of the peripherals using the bandgap request sample mode, then that will be the mode returned. Sample mode allows the bandgap to be active only when necessary to save on power consumption, static mode requires the bandgap to be active until no peripherals are using it anymore.
| bool REF_A_isBandgapActive | ( | void | ) |
Returns the active status of the bandgap in the REF module.
This function is used to return the active status of the bandgap in the REF module. If the bandgap is in use by a peripheral, then the status will be seen as active.
| bool REF_A_isRefGenBusy | ( | void | ) |
Returns the busy status of the reference generator in the REF module.
This function is used to return the busy status of the reference generator in the REF module. If the ref. generator is in use by a peripheral, then the status will be seen as busy.
| bool REF_A_isRefGenActive | ( | void | ) |
Returns the active status of the reference generator in the REF module.
This function is used to return the active status of the reference generator in the REF module. If the ref. generator is on and ready to use, then the status will be seen as active.
| bool REF_A_getBufferedBandgapVoltageStatus | ( | void | ) |
Returns the busy status of the reference generator in the REF module.
This function is used to return the buys status of the buffered bandgap voltage in the REF module. If the ref. generator is on and ready to use, then the status will be seen as active.
| bool REF_A_getVariableReferenceVoltageStatus | ( | void | ) |
Returns the busy status of the variable reference voltage in the REF module.
This function is used to return the buys status of the variable reference voltage in the REF module. If the ref. generator is on and ready to use, then the status will be seen as active.
| void REF_A_setReferenceVoltageOneTimeTrigger | ( | void | ) |
Enables the one-time trigger of the reference voltage.
Triggers the one-time generation of the variable reference voltage. Once the reference voltage request is set, this bit is cleared by hardware
Modified bits are REFGENOT of REFCTL0 register.
| void REF_A_setBufferedBandgapVoltageOneTimeTrigger | ( | void | ) |
Enables the one-time trigger of the buffered bandgap voltage.
Triggers the one-time generation of the buffered bandgap voltage. Once the buffered bandgap voltage request is set, this bit is cleared by hardware
Modified bits are RefGOT of REFCTL0 register.