Legend (explanation of the fields
in the
Manifest Table below)
Software Name |
The name of the application or file |
Version |
Version of the application or file |
License Type |
Type of license(s) under which TI will be providing software to the licensee (e.g. BSD, GPLv2, TI TSPA License, TI Commercial License). See Open Source Reference License Disclaimer in the Disclaimers Section. |
Location |
The directory name and path on the media (or in an archive) where the Software is located. |
Delivered As |
This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Software is delivered in. If the Software is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided. |
Modified by TI |
This field will either be “Yes” or “No”. A “Yes” means TI has made changes to the Software. A “No” means TI has not made any changes. Note: This field is not applicable for Software “Obtained from” TI. |
Obtained from |
This field specifies from where or from whom TI obtained the Software. It may be a URL to an Open Source site, a 3rd party licensor, or TI (if TI developed the software). If this field contains a link to Open Source software, the date TI downloaded the Software is also recorded. See Links Disclaimer in the Disclaimers Section. |
DISCLAIMERS
Export
Control Classification Number (ECCN)
Any
use of ECCNs
listed in the Manifest is at the user’s risk and without recourse to
TI. Your
company, as the exporter of record, is
responsible for determining the correct classification of any item at
the time
of export. Any export classification by TI of Software is for TI’s
internal use
only and shall not be construed as a representation or warranty
regarding the
proper export classification for such Software or whether an export
license or
other documentation is required for exporting such Software.
Links
in the Manifest
Any links appearing on this Manifest (for example in the “Obtained from” field) were verified at the time the Manifest was created. TI makes no guarantee that any listed links will remain active in the future.
Open
Source License
References
Your company is responsible for confirming the applicable license terms for any open source Software listed in this Manifest that was not “Obtained from” TI. Any open source license specified in this Manifest for Software that was not “Obtained from” TI is for TI’s internal use only and shall not be construed as a representation or warranty regarding the proper open source license terms for such Software.
Export Information
ECCN for
Software included in this release: Publicly Available
ECCN for
Technology (e.g., user documentation,
specifications) included in this release: Publicly Available
Manifest
See Legend above for a description of the columns and possible values.
Software Name |
Version |
License Type |
Delivered As |
Modified by TI |
|
|
MSP430F565x_MSP430F665x_Code_Examples |
1_00_00_00 |
BSD_EX |
Source |
|
Location |
|
Obtained from |
|
Credits
Licenses