FRAM Data Logging Mode
After the GUI is connected to the LaunchPad, click the Start button under FRAM Log Mode inside the Application Controls Panel. This puts the LaunchPad into the FRAM data logging mode.
The red LED1 blinks 3 times to indicate successful entry.
In this mode, the MSP430FR5969 enters Low Power Mode 3.5 and wakes up every 5 seconds to measure and record its input voltage and temperature to FRAM (visible each wakeup by the blinking green LED2).
To exit from data logging mode, click the S2 pushbutton on the LaunchPad. The red LED1 lights up shortly to indicate successful exit from data logging.
*Note: The GUI will disconnect from the LaunchPad automatically shortly after pressing Start. This is because the eUSCI module used for UART communication is switched off in LPM 3.5.