Simplelink Wi-Fi Toolbox Release Notes
Table of Contents
Introduction
SimpleLink Wi-Fi Toolbox is a cross-platform software kit, that provides all required tools for fast and easy ramp-up of the CC33xx family of devices. One of the included tools is Radio Tool.
Radio Tool is a tool for RF evaluation and testing of CC33xx designs, during development and certification. The tool enables low-level radio testing capabilities by manually setting the radio into transmit or receive modes. Usage of the tool requires familiarity and knowledge of radio circuit theory and radio test methods.
This is version 2.0.12 of the SimpleLink Wi-Fi Toolbox.
Release highlights
- Support Radio Tool for Wi-Fi
- Support Radio Tool for BLE
- Support INI Composer
- Support Logging
Documentation
Operating Systems Support
- Windows 10v 64bit
- Ubuntu 18.04 ( Higher ) 64 bit
Dependencies
This release was validated with the following components:
- XDS110 JTAG Debug Probe
- Chrome Web Browser Version 103.0.5060.134 (Official Build) (64-bit)
- Display resolution 1920 x 1080
Device Support
- CC33xx ICs:
- CC3301
Limitations
General Limitations
- The browser’s refresh button should not be used at any time while using the application.
- In case a Beagle Bone device is used as part of the CC33XX evaluation kit, the power connection must be disconnected from the Beagle Bone when using the Radio Tool.